News

Proven pedals for future truck generations
Leading European manufacturer KYOCERA AVX Components has launched the latest series of accelerator pedals for trucks – and they’re all set for whatever demands the

Change of AB company names
Our companies are being globally integrated into KYOCERA AVX Components starting on October 1st 2021. This process will go along with names changes in our

Novel power electronics for OnBoard Chargers, DC-DC Converters and Solar Inverters
Novel power electronics for OnBoard Chargers, DC-DC Converters and Solar Inverters Technology with a particularly high power density of more than 3kW/litre, enables among other

Position sensors supportASIL D capable assistance systems
Position sensors by KYOCERA AVX support ASIL D capable assistance systems for braking force control and recuperation KYOCERA AVX stands for the development and worldwide

SPINpad Technology
A High Speed Rotation Position Sensing Technology for next generation mobility.


Haptic Pedal
Our acellerator pedal reaches the driver directly, e.g. through vibration or knocking of the accelerator pedal.

The Electronic Hand Throttle
A direct communications interface with the driver – An integrated sensor continuously indicates the position of the electronic throttle grip, and this information is transferred

Pressure Sensor For Modern Hybrid Electric Vehicles
A special pressure sensor designed for use at the fuel tank of hybrid-electric vehicles is the latest development from the specialists for ceramic pressure measuring cells.

Battery Switch By KYOCERA AVX
For fast, safe and noiseless disconnection with high-performance electric vehicle batteries.